Part Number: OPA189
Other Parts Discussed in Thread: OPA205, OPA192
可以帮忙推荐一款放大器吗,要求如下:
1、VCM Common-mode voltage range,希望是(V–) + 1 ,(V+) – 1,越接近V-,V+更好
2、 0.1-Hz to 10-Hz这个范围的噪声要尽可能小,尽量像OPA189看齐
3、 Low voltage noise,在1khz的噪声密度要尽量小。
4、低温票
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,OPA189目前还处于量产阶段,还是可以继续使用的。
如果要找替代品的话,可以看下OPA205,0.1 ~ 10-Hz的噪声为0.2 µVPP。OPA 189的0.1 to 10-Hz的噪声为0.1 µVPP.。
1Khz的噪声密度为Voltage noise: 7.2 nV/√Hz。OPA189在1Khz的噪声密度为5.2 nV/√Hz。
另外,OPA205是轨至轨输出的,输入距离电压轨的范围为(V–) + 1~(v+)-1.4v.
总的来说,OPA205也是一看具有低输入偏置电路和低噪声的精度运放器件。
可以,OPA192也是一款输入偏置电流极低pA的精密运放,并且它是轨至轨输入输出。就是OPA192是一款比较老的芯片了,不如OPA205新:)