Other Parts Discussed in Thread: INA332
你好!目前我正在用INA332进行对接收到50mVp-p的超声波信号放大,但是INA332的输出完全没有响应!请麻烦帮忙分析一下。接收电路很简单,如附件所示!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: INA332
你好!目前我正在用INA332进行对接收到50mVp-p的超声波信号放大,但是INA332的输出完全没有响应!请麻烦帮忙分析一下。接收电路很简单,如附件所示!
Jeff,你好
请注意INA332手册中Page 10的内容,下面是一个参考电路,你可以先使用信号发生器测试你的放大电路。看看输出是否正常?
如果Vref=2.5V,与VIN-的电平就一致了,我电路图上的VIN-也是2.5V。那么A1的反馈回路上的10K电阻就无电流流过了!等于A1丢弃了!
june 你好
1,按照你的电路图的设计,ref应该要根据你最后一级的放大倍数进行相应调节,如上面提供的参考电路。当最后一级A3的放大倍数为2的时候,Vref的电压应该是 1.25V 。这样输出信号的中点电位则是2.5V。
2,按照参考电路所示,将信号发生器接入你的电路,看输出信号是否正常,得到20dB的增益。
3,另外,注意你的传感器的等效模型,是否包含直流成分?
你好!
1、我所需要的增益为500V/V。
2、我所用的传感器的等效模型并不包含直流成分。
3、INA332的两个输入端是不是需要比如2.5V的输入共模电压,才能正常工作?
June 你好
1、如果你的输入信号峰峰值为50mV,经过500倍的放大,将超出仪表放大器的工作范围。
你可以参考这个电路,增益 = 5 + 5*(R2 / R3),根据需求调整R2的大小。使用信号源输作为激励,试试是否输出正常:
2、请注意你的传感器(或者信号源)输出信号中包含的直流成分,有可能导致仪表放大器输出饱和;
3、不是必须的,这需要根据你的实际电路分析。根据你的输入信号幅值范围,要求的输出信号幅值范围,来设置合理的参考电压。