Part Number: TINA-TI


如上图,导入器件宏模型时提示行#110过长。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
上面回复内容为这个器件用文本打开后的源码,你可以复制下来然后保存为文本,然后将文件后缀改为.lib或.cir文件。
* TPH2502L1 OPERATIONAL AMPLIFIER "MACROMODEL" SUBCIRCUIT
* SUPPLY VOLTAGE = 5 V
* CONNECTIONS: NON-INVERTING INPUT
* | INVERTING INPUT
* | | POSITIVE POWER SUPPLY
* | | | NEGATIVE POWER SUPPLY
* | | | | OUTPUT
* | | | | |
.SUBCKT TPH2502L1 1 2 3 4 5
*
CPSR 85 86 159.2E-9
C0 22 8 18E-12
C1 22 _net0 1E-12
Cmr 12a 12 100.0E-15
CIN1 INPR INNR 0.6E-12
D3 21 18 DX
D2 18 20 DX
DIN2 INPa INP DX
DIN1 INP INPa DX
DC 5 53 DX
DCMP 81 82 DX
DP 4 3 DX
DE 54 5 DX
DCMN 83 81 DX
DLN 92 90 DX
DLP 90 91 DX
F3 10 _net0 VSRN 5.5
F2 10 _net0 VSRP 5.5
FPSR 7 99 VPSR 0.8K
F1 3 80a VCMP 1.0
FB5 8 99 VLN -5.5
FB1 7 99 VB 0
F0 3 80a VCMN 1.0
FB2 8 99 VC -5.5
FB4 8 99 VLP 5.5
FB3 8 99 VE 5.5e-9
E1 18 19 (11 12) 100
EPSR 14 15 (3 4) 75u
EP 16 _net0 (3 _net0) 1
E2 99 _net0 (99_a _net0) 1
ENSE 89b INN (88 _net0) 1
E16 12a _net0 (25 _net0) 1
Ecmr2 24 _net0 (2 _net0) 1
Ecmr1 23 _net0 (1 _net0) 1
EINN 71 99 (4 99) 1
E9 80b 99 (80 99) 1
ECMR 84 99 (INN 99) 1
EINP 70 99 (3 99) 1
E10 89a 99 (89 99) 1
EN 17 _net0 (4 _net0) 1
GPSR 85 86 85 86 100u
G1 22 _net0 11 12 0.0628318530717959
G0 8 _net0 22 _net0 0.0294053072376005
HLIM 90 _net0 VLIM 2.0K
IRP 3 4 6500e-6
I1 88 _net0 1e-21
ISS _net0 10 100u
II0 INN _net0 3p
VSRN 19 21 9.2
VSRP 20 19 9.2
V3 19 0 0
V2 15 0 0
VP0_PSR 85 14 -375.000u
VPSR 15 86 0
V1 13 89a 2e-3
V12 _net0 0 0
VCMP 82 70 550m
VLN _net0 92 19.2
VLP 91 _net0 19.2
VLIM 8 5 0
VCMN 83 71 550m
VAD 60 4 0
VE 54 4 820.00m
VB 9 _net0 0
VC 3 53 820.00m
V9 89 89b 50u
M1 11 13 10 10 PIN w=1.0u l=1.0u
M0 12 80a 10 10 PIN w=1.0u l=1.0u
R_ST2 8 9 500000
R_ST1 22 _net0 5412.45639115052
RL11 11 60 4.35E3
RL12 12 60 4.35E3
Rcm2 25 24 1E-6
RIN3 INNR 2 240
Rcm1 25 23 1E-6
R7 99_a 17 1E-6
R6 99_a 16 1E-6
R11 80 INP 1E-3
RO1 7 8 1E9
RIN1 1 INPR 240
R3 80a 80b 1.2E3
RIN2 INPR INP 240
RCM 84 81 1E3
RIN4 INN INNR 240
RN1 88 _net0 2.579E3
R18 INPa INN 6E9
** ends TP1282_7MHz_model
.MODEL DX D(IS=800.0E-18)
.model PIN pmos level=3 vto=-0.7 uo=200.0 tox=23.5n nsub=2.53e+16 nfs=1.8e+12 vmax=2.9e+05 eta=0.047 kappa=7.00 theta=0.139 delta=0.89 xj=0.14u rsh=1102.0 ld=0.225u cgdo=2.9e-10 cgso=2.9e-10 af=1.0 kf=2.6e-29 cj=3.1e-04 mj=0.370 cjsw=2.6e-10 mjsw=0.170 pb=0.360
.MODEL NIN NMOS KP=8.5E-6 VTO=0.7
.ENDS
我按照下面文档步骤编译的时候,确实出现了#Line110 is too long的error:

我找到E2E英文论坛中类似帖子链接如下,那边的工程师建议寻求DesignSoft support的支持。
如下支持链接:
Since TINA is a DesignSoft/TINA program, questions are handled by using the DesignSoft support page: http://www.tina.com/technical-support/ .