This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV321: 电压输出异常

Part Number: LMV321


LMV321IDCKR   当INPUT输入拉高为3.3V时,正常输出为3.3V,异常输出0.19V ,当INPUT输入拉低为0V时,正常输出为0V,异常输出0.14V,测量VCC电压3.36V。LMV连接测试图如下