Part Number: LMH6526
此芯片的输出方波是否可以过零?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您的问题我理解的输出信号电压是否过零是吗?
下面是LMH6526的输出架构,这是一款二极管驱动器,电流输出。 参考Table4,列举几种常用的不同供电电压下的最大输出电流以及内部FET的饱和电压。
以4.5V为例,5ohm负载下最大输出700mA电流,因此可计算输出电压3.5V,此时FET的饱和电压0.8V,可以得到供电电压至少3.5+0.8=4.3V,给4.5V供电,0.2V的余量。