This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2196: OPA2196做跟随器问题

Part Number: OPA2196

各位TI的工程师们,在使用OPA2196设计跟随器电路时,在运放的输出端与反馈端添加了一个限流电阻,用于限制预防的输出电流,详细的电路图见下图1,在设计中也使用了TINA进行仿真,在仿真过程中并未发现有振荡现象,但是在实际的电路中使用示波器测量输出端发生振荡,经过调试,在限流电阻两端并接了一个100pF电容,详细电路图见图2,振荡现象消失了,虽然问题得到解决,但是在上电过程中任由一小部分的过程现象,想请教一下TI的工程师以下问题:

1、当前用法是否会存在问题?

2、如果当前用法不存在问题,是否有条件改善过充问题?

3、是否有类似的使用电路推荐?

图1

图2

x 出现错误。请重试或与管理员联系。