Part Number: XTR117
Other Parts Discussed in Thread: TIPD126, DAC161S997, DAC161S997EVM

我的想法是:stm32的dac输出0-3.2V电压,使其XTR117能够输出4-20ma电流。已知压力传感器的采集端的采样电阻是100欧姆。不知道这个图是否正确?
另外我看手册上写到,IIN引脚输入的电压也有范围要求,从1V到最大值。那这个REF_5V大于1V是满足要求的吧。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: XTR117
Other Parts Discussed in Thread: TIPD126, DAC161S997, DAC161S997EVM

我的想法是:stm32的dac输出0-3.2V电压,使其XTR117能够输出4-20ma电流。已知压力传感器的采集端的采样电阻是100欧姆。不知道这个图是否正确?
另外我看手册上写到,IIN引脚输入的电压也有范围要求,从1V到最大值。那这个REF_5V大于1V是满足要求的吧。
您好,
STM32电路需要由XTR117的5V VREG供电,您需要确保完整的DAC+XTR电路电流消耗小于4mA。
使用2线电流变送器时,有几个注意事项:
1、在XTR117 两线电流变送器上,IRET电位是完整两线变送器电路的本地接地,其中,DAC或STM32必须由XTR117调节器供电,所有电路必须参考IRET GND。
2、两线电流变送器 XTR+DAC(在这里是STM32)的总电流消耗必须小于4mA,否则变送器输出信号将无法达到4mA的最小刻度输出。
另外我看手册上写到,IIN引脚输入的电压也有范围要求,从1V到最大值。那这个REF_5V大于1V是满足要求的吧。
是的。
我想加也给TVS管,可以直接并在10nf电容上是吧?
是的,下面截图是 TIPD126参考设计的截图:
https://www.ti.com.cn/tool/cn/TIPD126

很抱歉,漏掉了您的这个帖子,今天才看到还没有回复。
我的stm32的电流消耗肯定会大于4ma,这该怎么办了,
如果还是使用两线的话,那么只能使用本地电源然后隔离供电了,具体见下面FAQ:
[FAQ] The minimum output current of my 2-wire 4-20mA transmitter is greater than 4mA.
Can I use a 2-wire transmitter with a sensor or microcontroller that uses its own supply?
我刚看了一款新品DAC161S997是电流型的。我没看到关于输出电流精度的描述。
datasheet中关于输出电流精度的描述如下截图,您可以主要看TUE参数:

我设想这样使用这款芯片,不知是不是对的
您可以使用这个芯片,但是这个也是需要加隔离的,您可以参考 DAC161S997EVM 原理图,在其用户指南中有提供:
https://www.ti.com.cn/cn/lit/pdf/snlu146
更多关于4-20mA电流环的应用信息见下面FAQ:
[FAQ] Designing with 4-20mA current loop transmitters (XTRs): FAQ links