Part Number: OPA551
Other Parts Discussed in Thread: OPA564
我用DA芯片再加了一级运放AD8065输出1 - 10V,40 - 60KHZ 的正玄波,然后用OP551扩流后再驱动后边的MOS管IRFP250(或2SK1058),用multisim仿真时可以(正玄波输入,正玄波输出,电流可以达到260mA),但不知道实际电路效果会怎样,有关OP551驱动功率MOS管的使用麻烦您给些建议,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,OPA551 输出持续性电流为200mA,您需要260mA输出吗?下面是OPA551的SOA(Safe Operating Area )曲线。可以看到,安全操作条件下,最大可持续输出电流为200mA。 并且随着Vs-Vo的增大,最大输出电流随之降低,datasheet中380mA指的是瞬态峰值。

所以如果驱动MOS需要持续性输出260mA的话, 建议是换输出电流更高的芯片,比如OPA564. 并且驱动电流的应用,建议是参考OPA564 Figure54的应用,在输出端和电源端加上肖特基二极管以及TVS,防止电压过压,反极性保护等。