This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA227: OPA227: OPA227+FZT851驱动LED,为什么LED电流达到1A左右就不能继续上升了?

Part Number: OPA227

我用官方电路图驱动15W的LED,期望得到至少2A的电流。按照说明,可以满足要求:

刚开始只能达到最大0.8A电流,后来我改成Vs=+5V供电,LED电流可达1A左右,但是当我想继续提高电流,将Vs接到12V时,FZT851三极管马上烧毁。

想知道:

         1、是什么原因电流上不去?电流不应该和Vs有关啊,不应该由Vin和电阻决定吗?

         2、还有为什么三极管烧毁,难道是功率太大?

         3、或者有什么其他运放电路方法实现LED大电流恒流调光吗?(模拟调光)