This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
由于altium designer没法更好的显示原理图,所以用TINA做了这个原理图,请大家帮我看看有什么问题
这是我自制的pcb
测试的时候出现两个三个问题,第一个问题就是ths3001和buf634级联的地方那个Ro的作用,buf634的输入阻抗不是M欧姆级的吗,但我改变Ro的阻值,发现Ro能分得很大一部分电压,很奇怪。。。
第二个问题是:我在没加50欧姆负载RL的时候,ths3001输出2.8V峰峰值,10Mhz正弦波,放大十倍,输出一切正常,但是我加上50欧姆负载后,波形严重失真了,请问问题出在哪里
第三个问题是:buf634的1管脚和4管脚间连的那个电阻到底能不能拓展带宽,为什么当阻值很小时,静态电流会有几百毫安。。。