This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OPA564-Q1的带宽(请大侠指导)

Other Parts Discussed in Thread: OPA564-Q1

烦请诸位大侠赐教!

我打算用OPA564-Q1做电流放大,为了保证总谐波失真最小,据数据手册第10页figure17,将OPA564-Q1增益设为1;从前级DAC(经带通滤波后)输入OPA564-Q1的信号频率范围是1k~100kHz,输入电压峰值10v(即峰峰值+-10v,其中DAC为20位,最大支持+-15v的电压峰峰值输出);OPA564-Q1的输出负载为感性负载(直流电阻4欧,电感200u),注:在10kHz以下负载阻抗较小,系统会对应减小DAC输出电压幅值,使负载电流不大于1A。

从数据手册第11页figure22,只能看到频率小于20kHz的THD+N指标,请问从20kHz~100kHz这个频段的THD+N指标是多少呢如果没有可靠的数据,是否可以根据OPA564-Q1的技术参数(如增益带宽积17MHz,满功率带宽(在10VPP 时) 为1.3MHz)进行大概推算呢? 我希望20k~100kHz范围内THD+N能达到75db以上。从figure22可以推算在20kHz以下,工作条件如上,THD+N可以达到0.003%(90db)。

烦请大侠们帮忙!万分感谢!