Other Parts Discussed in Thread: PGA281
我的信号链是:前放(仪表放大器)—>带通滤波—>PGA281—>差分ADC。前放固定增益100倍,经过带通滤波后,信号电压幅度在80mV~2000mV。考虑到尽量使ADC满量程工作以提高有效位数,想加入可编程增益放大器PGA281做二级放大。
(1)请问可编程增益仪表放大器PGA281的输入可以是单端吗?还是必须是差分? 因为见数据手册25页图51上有单端应用的例子。
(2)如果可以是单端输入(比如同相输入,反相端接地),还能起到仪表放大器的共模抑制作用吗?
(3)请问此信号链中使用PGA281是否合理?还是应该使用固定增益二级低噪放大器更加合适呢?
(4)如果使用PGA281,增益等级会取自1倍—32倍,在此情况下PGA281是否满足100kHz的带宽要求(数据手册上PGA281增益带宽积为6MHz当Gain > 4 V/V)?