Other Parts Discussed in Thread: INA132
如下图,简单的霍兰德恒流源
一个批次上电后INA132输出脚6为0V,OPA140的3脚0.7V,6脚输出直接4.3V,输出饱和。
通过更换不同批次的的INA132与OPA140,问题可以解决,但是OPA140通常需要更换2至3个才能正常,电阻R12下端最大1.25V。
通常更换OPA140后,第一次上电,示波器抓取波形如下
紫色为3脚输入,青色为6脚输出,恒流源负载为电容,青色斜坡爬升是对的,但是输出是方波。
请帮忙分析:
1.电路是否正确?
2.异常时,紫色超过1.25V运放输出达到正轨饱和,可以理解为超过共模输入范围,但是低于1.25V时,为什么不跟随。碰运气更换的OPA140就跟随的很好,紫色斜坡很直。
3.OPA140很脆弱吗?感觉问题很多。