你好。
文档中提到XTR300有三种配置模式:
- Voltage Output Mode
- Current Output Mode
- EXTERNALLY-CONFIGURED MODE
在EXTERNALLY-CONFIGURED MODE下,只是将IMON和IAOUT独立开来,以便同时监视,还是有其他区别?
另,EXTERNALLY-CONFIGURED MODE的外部反馈依据什么进行搭建反馈回路?
thanks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在Externally Configured Mode下,OP-AMP和IA是两个独立的器件,可以把这个芯片看成集成了运放和仪放的芯片。外部的反馈就是运放自己的反馈,就是正常的运放负反馈电路的搭建方法。
意思就是说可以独立的使用OPA 和IA 两个运放,具体应用我没看到。
In voltage output mode, the signal output current can be observed and measured at I-MON with 0.1V/mA
(with R9 = 1k).
In current output mode, the signal output voltage can be observed and measured at IA-O with 0.2V/V (with
R10 = 1k).
These output pins can be connected together to form a general monitor output, because they are
internally multiplexed