This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问一下,除了分压,使用运放如何实现0-5V到0-3V的范围转换?
请问是直流信号,还是交流信号?
是直流信号
反向放大电路,0-5V转换成+-1.5V,偏置1.5V,从而得到0-3V。。。
也可以看看PGA281,有小于1的放大倍数
使用运放如何实现0-5V到0-3V的范围转换:放大倍数设置为0.6就行了,有很多增益小于1 可以稳定的运放,且这是个直流信号
标准答案:电阻分压+运放跟随。