Other Parts Discussed in Thread: OPA1611, OPA890, LMH6559, OPA354, OPA353
请问有电压跟随器的产品吗?产品性能怎么样?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI有很多单位增益稳定的运放产品,适合做电压跟随,比如OPA1611,OPA890等这种,不知你的具体要求是什么,比如供电电压,带宽等的要求
这个误差受很多因素的影响,比如像大家提到的输入电压噪声,输入失调电压(datasheet中都有随频率变化的曲线),温漂,输入偏置电流遇到电阻网络引起的电压误差等,所以我们在选择时尽量选择精度高的,单位增益应用时,选择单位增益稳定的运放产品。
我想跟随15M的2.8Vpp的正弦信号,供电+3.6V,请问什么芯片适合
请问LMH6559能达到如下性能吗,我的输入信号是2.8VPP的15M正弦信号,供电电压+3.6V,单电源供电,负载200欧姆
你好,请问我的输入电压是2.8V峰峰值的15M的正弦信号,单电源供电电压+3.6V,要求输出2.8V峰峰值,负载为200欧姆,请问哪款运放或者buf适合我,楼上的说LMH6559根本不行啊,他的输出摆幅<2Vpp,害得我费了好大的劲
不好意思啊,忽略了你的电源供电是单电源3.6V,可以使用OPA353,OPA354.对上次的回复表示抱歉啊
请问我的供电电压是单电源+3.6V,如果我使用升压芯片将+3.6V升到+5V或者更高,那么我能选用的作为跟随器的运放就多多了?
可能相对来说会多一些, 因为你单电源供电的话,如果产品不是轨至轨输出的话,输出跟随输入的能力是有限的,可能只能再电源轨的1点几V之内,所以如果不采用升压的话,carter帮选的OPA353,354是能满足你的需求的,因为这两款是轨至轨输入输出。