This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用THS3001和THS3091做功率放大器,仿真可行。焊的电路用信号源和示波器测试,可以输出10Vrms(15V供电,由于芯片供电饱和,最大输出也就只能是9.8Vrms的样子,真正到10Vrms时波形上下都略微截止)。
接入到系统中时,实际电压上不了6Vrms,也就5Vrms附近,再加大电压波形完全就乱了,此时容易烧片子。不敢往上面加大电压,怕烧了片子,已经烧了5、6片了。系统中它的前级是OPA690放大电路输出端接了个50欧的电阻。
为什么示波器接入信号可以到10Vrms,但是接入到系统中就只能到5Vrms。
xiaohao tao 说:因为在前级放大器后面是串联了一个50欧的电阻输出的,相当于模拟信号源的内阻,但它就是不行,接了电压跟随后就行了。
是不是后面没做阻抗匹配的原因,功率没有最大传输。
zhiwei Liang 说:因为在前级放大器后面是串联了一个50欧的电阻输出的,相当于模拟信号源的内阻,但它就是不行,接了电压跟随后就行了。
是不是后面没做阻抗匹配的原因,功率没有最大传输。
[/quote]
应该是前级放大器后串的50欧姆电阻,产生了楼上所说的负载效应,导致了信号传输不止有信息的交换,还有能量的损耗交换。减轻负载效应的方法,在截图附件上,有。