This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

xtr111限流问题

Other Parts Discussed in Thread: XTR111

按照datasheet  Figure 36. Basic Connection for 0mA to 20mA方式连线。

1 Q1使用2SJ637  Q2使用9012 系统工作正常。

2输入为DC 0.8-2V Rset=2K ,输出4-20mA正常。

在20mA时Q1发热量大,Q1表面温度60摄氏度,4mA时温度30摄氏度。

偶然在20mA工作15分钟,Vin正常,电流输出100mA,(未出现限流),立即断电上电后依旧输出100mA,待30分钟后上电发现恢复正常。

请问导致xtr111输出电流不正常的原因?是否跟Q1工作温度有关。

  • 由于晶体管的电气特性差异很大,它管理着整个输出电流的量程,建议您更换Q1的型号,采用datasheet上推荐的几款型号重新验证是否正常。

  • 能否给出PCB设计图,如果外置的扩流BJT位置不合适会导致XTR111被加热,从而会对整体新能影响较大。但是你处采用Figure-36的设计,输出电流过大的话Q2会动作关闭输出。建议,检查Q2为何没有导通。15ohm电阻两端电压差是关键