Other Parts Discussed in Thread: THS3001, THS3091, THS3092
一般用集成运放做功率放大器时,网上文档十之八九是用THS3091并联增大功率,前面是THS3001作缓冲的那种。但是THS3001和THS3091都是电流型反馈运放,输出电流都很大,满足功率放大的要求。其他性能也都相近。但我疑惑的是为什么都选择用3091而不是THS3001。希望大神解决我的疑惑。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谁说THS3001并联做输出缓冲级不好的?安捷伦堪称最经典的任意波形发生器33220A里面的最后一级(保护电路除外),就是采用的四片THS3001并联的方式。每片100mA,一共400mA(当然实际肯定难以达到400mA)。
实际中,THS3001跟THS3091还是有一些区别的。如果仔细研究,在某些场合区别还不小。
THS3001供电电压最高正负16V,3091只有正负15V。别小瞧这1V的差距。本人曾经遇到一个设计需要产生30V峰峰值,我们就通过研究THS3001内部的工艺结构,觉得给他正负18V,只要保证散热良好的情况下也问题不大,因此顺利的达到了要求(当然正式的产品可不能这么做)。如果换成THS3091,估计3091会挂掉。
THS3001输出电流最大只能到100mA,而3091可以到250mA。
另外,THS3091的一大特点是总谐波失真特别小。THS3091的双运放版本,THS3092,用来做音频耳放的输出级,一点都不逊色于知名大厂家的千元耳放。
下面是安捷伦的任意波形发生器33220A的内部电路图(输出级部分),供你参考: