Other Parts Discussed in Thread: TLC2652A
我经常会设计一些放大倍数非常大的放大器网络,经常会达到100dB以上,采用多级放大的话,经常会遇到运放进入饱和区的情况,采用逐级的衰减网络的话,还是不能从根本上解决这个问题,有没有什么方法可以从根本上消除设计时的自激问题,以及运放进入自激状态后怎么消除自激问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
100dB相当于一万倍,必须采用多级放大,遇到饱和可能是前级放大器的输入偏置电压经过放大后产生的,可以考虑用零漂移的运放,如TLC2652A
各级间的信号屏蔽也很重要,应当注意一些意想不到的反馈回路。
100dB的放大倍数已经和运放的开环增益相当,如果使用集成运算放大器实现100dB的V-V增益肯定是不现实的。不过如果是I-V跨导1M还是比较常见的。如果是跨导放大,那么需要做好相位补偿来消除自激振荡。
能否能说说是什么类型的信号源?如果信号是放大后需要进行采样,是否可以考虑放大一个几十倍后使用一个高精度ADC来采样。