This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教

你好:我想设计一个音频放大电路,由MIC(咪头)采样5--10微伏噪声,采样那款放大器可以放大到3伏?后面用16位AD接MCU处理噪声分析!

谢谢

  • 楼主你好!

    根据你的实际情况,需要将信号放大120dB,而一般的放大器的开环增益在音频范围内最高也就到120dB,所以楼主需要做多级放大。

    因为信号大小只有5~10uV,所以第一级放大器需要选用低失调电压的放大器,最好比5~10uV低,而且噪声也要低,否则信号就会被噪声淹没。

    前级的放大倍数尽可能的高,这样才会让尽可能少的后级的放大器的噪声被放大。

    楼主可以综合考虑使用3~4级放大。注意,只有将信号放大到mV级别之后再使用100MHz以上GBW的放大器。因为这类的放大器一般噪声以及失调电压会使得百uV级别的信号被淹没。