This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4820问题再问!



你好!

     谢谢(秋之初)您的答复!我是在用这个放大器做微光探测前端的V/I转换,探测器输出端的电流大概在1nA~10nA之间,频率为100MHz的正弦波。运放的第一级为buffer,所以按照电压跟随器方式搭接,是不是需要探测器输出的电流转电压的电阻提高到1.3V以上这个电压跟随器才能够正常工作?在100MHz下该运放用作电压跟随器应该如何搭接?

     实际搭接电路时由于没有很好的信号源,所以先使用20K做了测试,结果出现第二个现象。

     贵公司有没有更好的适合我这种情况使用的运放,请推荐,谢谢!!

     附件为我的电路图。

新建 Word 2007 文档 (2).docx