Other Parts Discussed in Thread: VCA821, OPA695
use TI's parts vca821 & opa695
performance:
增益可调范围0~60dB连续可调
-3dB带宽(fL~fH)13K~120M @60dB增益
1dB平坦度100k~90M@60d增益(100k为起始测试频率)
峰峰值噪声< 80mVpp @ 60dB
输入信号范围1mVpp~20mVpp
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不好意思各位,由于长期没有关注论坛所以没看到你们的回复,深感抱歉,上面是我创建的小号。具体的设计方案是这样的:前级采用了ERA-3SM+射频放大器,噪声系数在2~3dB左右,增益为21dB。中间级采用了VCA821压空增益放大器,它的主要特点是高带宽和衰减特性,主要是用vca821来衰减前级和后级的增益(具体性能可以好好参考一下数据手册)。后级采用opa695电流反馈放大器,作驱动负载的作用。这个方案还是存在缺陷的,个人认为主要的局限是运放在高频大信号输出的情况下谐波特性比较糟糕。本人才疏学浅,讲的不对的地方希望大家多多指教,谢谢!