This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
多谢。新手,请包涵。再请教一点,我可以通过单片机DA输出到VR这个地方,然后直接控制VCA810的增益从-40dB到+40dB变化吗?如果不可以,请问要怎么用VCA810来实现呢? 谢谢!
根据我的调试经验,这里就是如楼上所说的检波二极管,看是硅管还是诸管,导通电压不一样。在VCA810里有个控制放大倍数的公式,用一片DAC来输出-2V~0V的电压即可控制增益放大。但是DAC输出的是正电压,需要经过一级反相器来得到负压,注意是双电源供电哦,也不要用单电源的运放。如果是单电源供电,就得考虑所有器件的供电问题了,需要加偏置电压。这个另当别论。不要用单电源供电即可得到负电压的。然后,如果楼主要做AGC的话,那么反相器的运行建议使用高阻输入的,比如TL081,,输入电阻越高越好。好吧。太罗嗦了,主要是对810感情太深了。。哈哈
我此前其实是做了一个首先用OPA657放大光电流后面再用VCA820手册里面的AGC loop做的一个放大,把光脉冲放大到单片机可以捕获的电压脉冲。存在好些问题,首先是VCA820的AGC loop输出啊有一个比较大的偏置,其次,这个AGC loop工作起来发热很严重,我也不明白怎么回事,另外就是对于这种双电源供电的微弱信号放大的电路,电源供电方案用什么比较好啊?我开始用电荷泵,但是发现电源文波太大了,电路受干扰很严重。后来只有用了LDO。现在用TINA仿真试了一下VCA810,感觉VCA810电路输出会比VCA820好。所以想换掉电路。但是发现论坛了有人遇到了这个问题:http://www.deyisupport.com/question_answer/analog/amplifiers/f/52/p/30187/236606.aspx#236606,不知道做出电路我是不是也有这样的问题,所以还想问问VCA810手册中的RSSI Port是什么个作用,要怎么处理;手册中VCA810的AGC loop中-V直接接电源-5V行不行?
对电路不是特别熟悉,我的问题可能有点多了,希望您能解答。非常感谢!
非常感谢你的解答。如果温度上升二三十度的话,那确实和我板子上的情况差不多。芯片摸上去烫手,但是不至于特别烫。请问一下啊这个种功耗估算的方法有什么手册和资料可以参考学习的?我其实不太明白这个电路功耗的估算。对于VCA810的话,RSSI是接收信号强度指示,那是不是应该不会有这样的问题:(下面是另一个人发帖说的)
大家好,今天调试VCA810 datasheet中的AGC电路,调了好长时间偶然中才出来结果:示波器1通道接RSSI Port ,示波器2通道接输出,这样的话才能出现结果,现象稳定。。但是把通道1的探头拿掉就没结果了。。。。个人认为是RSSI Port中有电流流不走,聚在VC段使VC的电压为正,使用示波器接上RSSI Port后电流流入示波器,VC段为负,信号放大正常,实现AGC。于是我接了一个1M的电阻在RSSI Port和地之间,但是结果还是不行。。。不知道datasheet的电路图中RSSI Port的真正作用是什么,上面问题怎样解决,求大神指点。。。。谢谢了!!!
您好。这个接收信号强度指示,是不是输出为了给系统中其他电路部分比如MCU指示现在配置的VCA810的放大倍数的情况?在实际使用中不接也是没有任何问题的?