Other Parts Discussed in Thread: INA2331
请问INA2331的Shutdown管脚是否可用,在DATAsheet中没有相关的描述。我在实际的硬件测试中将Shutdown管脚接地,INA2331并没停止信号放大。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: INA2331
请问INA2331的Shutdown管脚是否可用,在DATAsheet中没有相关的描述。我在实际的硬件测试中将Shutdown管脚接地,INA2331并没停止信号放大。
kerwin
你好!
shutdown引脚是可以工作的。
能提供你的电路图吗?在你的电路中INA2331是怎样供电的?
你好!
INA2331的正常工作电压(V+ 头 V-)为 2.5V 至 5.5V, 你的设计中供电为正负3.3,已经接近了极限供电电压了。
如果正负供电的话, 例如以 正负 2.5V 供电, 那么我们要将shutdown电压设置在 -2.5 至 -1 之间:

INA2331的输入为300KHz、20-40mv的差分信号,该信号来自超声波发送接受一体探头。同样需要ShutDown功能,在单3.3V电源供电的情况下,INA2331能不能对该差分信号进行放大,放大之后有没有负半轴的波形?如果不行能否提供一种替代方案。