1:恒流源部分电路正常,压力传感器3-1端有20mv的压差。
2:实际测量LMV774芯片7-8管脚间压差为0V,按照设计应该为60mv
3:实际测量LMV774芯片1管脚对地间压差为0V,按照设计应该为600mv。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1:恒流源部分电路正常,压力传感器3-1端有20mv的压差。
2:实际测量LMV774芯片7-8管脚间压差为0V,按照设计应该为60mv
3:实际测量LMV774芯片1管脚对地间压差为0V,按照设计应该为600mv。
kerwin:
你好!
请问传感器pin1 pin3 分别对地的电压值是多少?
LMV774的供电是怎么样的?
LMV744是四运放,这里只用到三个运放,剩下一个是如何处理的?
PIN3对地电压3.263V;PIN1对地电压3.243V。
LMV774 是 输出轨至轨 运放, 输入并不是轨至轨。当3.3V供电的时候,你的输入信号已经超过了运放的正常 输入范围。
另外,在3.3V供电的情况下,让输入信号的共模电压在 1.65V,可以最大地利用运放的输入输出范围:
在正常的大气压力下,压力电桥4-2端电阻为4K。参考该传感器的官方资料要求电流为1.5mA,所以PIN1与PIN3的共模电压正常情况下达到6.3V。可是我的电源电压只有正负3.3V以及20V。请推荐一种改进方案,或者推荐一个替代LMV774的四通道运放。
衷心感谢各位提供的帮助!
你好!
提供仪表放大器的供电电压,可以扩大信号输入范围,进而可以提高传感器部分的激励电压值,提高灵敏度,供你参考:
FYI
附件是参考电路图
调节图中参考电压的电压值,可以设置最后信号输出的中点电平值。