Other Parts Discussed in Thread: INA333, INA826
刚刚学习运放这一块,很多东西理解不到位,所以来请教一下。
现在需要将一个传感器的信号放大输入到ADC,传感器信号Vpp约500mv,能分辨出30mv的信号来放大,信号是100KHz,要放大到10V输出。
还有由于应用的要求,需要将传感器信号减去100mv后再进行放大,这个是用偏置电路实现吗?
请大家给点建议,指导下运放的选型和电路搭建的思路,谢谢啦!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个30mv分辨是我描述错误,请大家忽略掉吧。
另外需要的精度要相对高点,有什么运放信号可以推荐吗?
虽然很多运放就可以实现,不过,不确定您前级传感器的输出阻抗的大小,以及还要做100mV偏压,我觉得可以考虑用仪表放大器,
根据系统供电情况,低压可以考虑INA333,宽压可以考虑INA826等等。。。
感谢你们的建议,现在打算用INA826试一下,在实现我的需求的设计中要注意点什么呢?
另外看了INA826的文档,当中的提供偏置电压返回路径该怎么理解呢,在电路中要怎么样实现吗?