This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运放双电源供电和滤波

Other Parts Discussed in Thread: OPA4170

运放在采用双电源供电时,该如何做好电源的滤波。一直搞不清如何选择滤波电容的容值大小,耐压值和电源电压的关系。

如下图中,我采用的是±15V给OPA4170供电,滤波电容采用的是10uF/25V(AVX钽电容)和0.1uF(TDK)组合滤波,但在测试的过程中,偶尔会有钽电容爆掉的情况发生,对系统的稳定存在很大的影响。对此,各位有什么好的建议?

  • 运放的电源,应该接100ohm和1uF的组合体。如图示:

     

  • 关于电容爆掉的问题:

    国产的钽电容成本可能只有国外的钽电容的1/4,但他们的实际耐压值经常不到标称值的一半,而且也经常容值虚标。建议使用原装进口的优质钽电容,或者更换更高耐压值的国产钽电容(这两种方法其实付出的成本是相似的)

  • AVX飞国产品牌。http://www.avx.com/

  • 如果选用国产钽电容,那么最好选用工作电压3倍耐压值的电容。

  • 请问有进口的优质钽电容推荐吗 ,大致有哪些公司生产钽电容。另外问一下,钽电容和无极电容(比如TDK)哪种滤波效果好一些?

  • 楼主你好,钽电容很多公司都生产,有你所用的AVX、KEMEX、三星、NEC、威世等公司都有相关的产品。AVX跟KEMEX的因为品牌大,所以国内的假货很多。

  • 关于电源滤波,我觉得使用铝电解+无极电容即可。无极电容不要光使用104就完事,最好根据运放的工作频率,选择合适的电容。如果工作频率高于1M,那么10nF左右的电容是必需的;如果工作频率高于10M,那么1nF的电容也是必需的。

  • 滤波电容瓷片电容,推荐使用NP0电容。温度稳定性好。其它电容CBB电容也不错。一般电解电容不用于滤波器。像钽电解电容,它不能接负向电压,如果电压反向一般很容易爆。下面是常见电容的比较,希望对你有帮助。

    电容类型  Capacitor types Capacitance range Accuracy Temperature stability Leakage Typical Dielectric Absorption
    电解 Electrolytic   0.1 uF - ~1 F   Very poor  Very poor   Poor   high
    陶器 Ceramic   10 pF - 1 uF   Variable   Variable   Average   NPO <0.1%
    Tantalum   0.1 uF - 500 uF   Poor   Poor   Poor   high
    云母 Silver mica   1 pF - 3000 pF   Good   Good   Good   >0.003%
    聚酯 Polyester (Mylar)   0.001 uF - 50uF   Good   Poor   Good   0.3% to 0.5%
    聚苯乙烯 Polystyrene   10 pF - 1 uF   Very good   Good   Very good   0.001% to 0.02%
    聚碳酸酯 Polycarbonate   100pF - 20 uF   Very good   Very good   Good    
    聚丙烯 Polypropylene   100pF - 50 uF   Very good   Good   Very good   0.001% to 0.02%
    聚四氟乙烯
    特氟龙
    Teflon   100 pF - 1 uF   Very good   Very good   Very good   0.003% to 0.02%
    玻璃 Glass   10 pF - 1000 pF   Good   Good   Very good    
    陶瓷 Porcelain   100 pF - 0.1 uF   Good   Good   Good