lmp2021单运放,单电源供电,能否设计成差分输入?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
单电源供电的局限性就在于对负半轴部分的信号无法处理,并且不是轨至轨输入的话,在地电平附近的信号也是无法处理的,所以如果差分输入的话,只能双电源供电。
应用场景是检测电流,通过采用电阻转换成电压。对负半轴信号不用处理,只是单电源是否对低电压信号放大有影响,最低电压大概100uV左右。
如果用双电源,输入单电源电压是12V,TI有什么芯片推荐转换为双电源?
如果像您说的最低电压 在100uV左右,那么单电源供电,对运放的选择是个考验,要选轨到轨的,但是轨到轨实际中对电源轨还是有一定压差的。。。
现在的运放工艺,可以做到几个uV级,很多。。。
检测电流的话可直接使用TI的电流检测运放产品,不知你需要检测的电流是多大的?打算采用多大的电阻?放大倍数为多少,对精度有什么要求?你可参考下INA225,INA300这类电流检测产品。
检测电流跨度大,uA至百mA级别精度为0.01。运放输入端最低电压为100uV左右,放大后在5mV左右。INA225,INA300的Vos太大吧。lmp2021在单电源下是否可以输出5mV左右?