我用OPA551构成双运放的恒流源,如图所示。供电电压±23V,R1=R2=R3=4=10K,R0=1K。设计要求是输入电压范围-3~3V,转化成-3000~3000uA输出电流,我接了一个5K电阻做负载RL,理论上当我输入3V直流信号时,RL可以达到15V,在A2的输入范围内,A1输出电压应该是18V,也在输出范围内,可是当我用250Hz正弦波输入时,发现当信号高于1.5V或小于-1.5V时信号就不能正常输出开始变形了。而直流时3V还是可以正常输出3000uA的电流的,我看了OPA551的输出幅值与频率的表格,明明是符合我的设计的,可我测试了一下发现OPA551输出上限在10V以下,如图。那么我的情况是怎么回事?