This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7322电压放大的问题

Other Parts Discussed in Thread: LM7322

您好,我使用LM7322做电压放大,电路如下所示,

供电电压VDD=12V,VSS=GND,放大电路为同相放大,放大倍数可以根据电路计算得到为15倍,那么当输入电压为0.3V的时候,输出就应该是4.5V左右,但是实际上电路输出电压大小却接近于供电电压,差不多11V左右。我连续换了两个芯片都是这个结果,真的很奇怪!

然后我就开始怀疑难道这块芯片是不可以放大电压的,但是这个怎么可能呢!!看了好几遍数据手册也感觉没有问题,然后我用TINA_TI进行仿真了,结果是没有问题的,如下图:

输出的节点电压为4.34V,接近了4.5V。

可是为啥实际情况下就是不能输出正确的电压呢,真的是百思不得其解啊,这个项目真的非常急,希望得到大家的指点,谢谢~~