THS4130全差动放大器是否可以正负3.3V供电?
参数标称:VCC = 5 V Single Supply to ±15 V Dual Supply

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
THS4130全差动放大器是否可以正负3.3V供电?
参数标称:VCC = 5 V Single Supply to ±15 V Dual Supply

kerwin
你好!
可以的,手册的意思是,单电源供电可以接受4 ~ 33V, 双电源供电±2 ~ ±16.5。 其实是一个意思,V+ 至 V- 压差 在 4 ~ 33V 都可以。