This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA309的EEPROM的问题请教

Other Parts Discussed in Thread: PGA309

现在用的PGA309和24LC16BE(PGA309应用的典型电路4-20mA输出),在校准完成之后零点输出4mA,断电放一段时间,再上电有的时候电流输出值变成0.6mA,然后读取eeprom的值发现程序的标志位变了,原来正确的值应为5449,更改之后的值就不一定是什么值了,请问有没有遇见过同样的问题,可能产生这种情况的原因在哪啊?

  • 24LC16BE WP pin有接高电平吗?

  • 您好,24LC16BE的WP引脚没有接高电平,而是接的地;如果接高电平的话就不能写数据了,这个引脚是不是写完数据之后必须接到高电平啊?有没有其他的改善措施啊?

  • 可以考虑

    1. 焊接前烧些数据,电路板上始终Pin WP = High.
    2. 板上作条线,写时Pin WP = Low. 写完后Pin WP = High.

    工业场合的任何干扰可能会对I2C总线产生毛刺脉冲,符合EEROM写入时序的话就会产生误操作。如果要查找准确原因,请用示波器捕捉发生错误时的波形分析。

  • 你好,最近我也在搞PGA309evm,遇到了点问题,能请教下您么,我的qq是499521179,能留下联系方式么

  • 你好 我也在做PGA309,刚着手,可以交流下么,我的QQ:1920993458

  • 请问你解决这个问题了吗?我现在也遇到了5499变成其他的值数据出错
x 出现错误。请重试或与管理员联系。