This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA857: OPA857的最大输入电流问题?

Part Number: OPA857


【OPA857输入电流大小问题】

根据OPA857 datasheet指出,OUT端口的输出摆幅为0.6~1.9V

而由Functional Block Diagram可知,假设增益为5kΩ,OUT = Iin * 5kΩ + 1.83,且OUT的最大值为1.9v,即Iin * 5kΩ + 1.83≤1.9,则输入电流Iin ≤ (1.9 – 1.83)/ 5kΩ,Iin ≤ 14uA

所以意思是OPA857输入电流超过14uA就饱和了吗?

下图为OPA857的仿真图,当输入电流超过14uA之后,得到的输出电压就饱和了,OUT 保持在1.895V。