这是OPA690数据手册中典型电路,我按照其电阻值的设置,焊接了一个电路。由于我们实验室的信号发生器的输出能力不行,输入端的50ohm的电阻会将我的信号幅度拉低,我将其换成600ohm左右的电阻,店里工作正常。
但是放大倍数只有两倍,能不能制出5倍或者10倍的放大电路?这阻值如何设置?我试过了很多的阻值都不行!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入端的50ohm是和信号源的阻抗匹配,为什么要换成600ohm?如果担心将信号幅度降低,可以不加。
另外,输入信号幅值多少?注意放大5倍或10倍是由于输出饱和导致不能正常输出。
楼主,是这样的!50欧是做匹配的,如果考虑功率最大传输,这种匹配是必要的。但是输入信号幅度(指信号进入运放输入脚的幅度,而不是信号源输出幅度)会降低一半,所以,你所谓的接上600欧后放大倍数减小,你应该测出输入引脚信号,测出输出引脚信号来比对。不能用输出信号除以信号源信号来算放大倍数。不知道楼主用的什么方式。。 如果计算方法正确,在确认电路无误后请尝试换一个芯片,我之前也是被THS3201整了一天,说好的5倍,只有两倍,后来新的芯片到了,换上去才发现芯片坏了。一般手册上的数据还是比较可靠的
哦,原来楼主说按照典型电路参数只能放大2倍,我还以为按照原理图电路结构自己焊接的10倍阻值参数还是2倍呢!
是这样的,我看了opa690是电压反馈运放,一般是没有特定放大倍数的推荐参数值的,只有电流反馈才有推荐阻值。电压反馈运放的取值是比较宽泛的。
1.楼主说Rf增大会自激,理论上是不应该的,不过你依然可以通过在Rf上并联一个pf级的电容,来改善一下。
2.楼主第二个问题,40.3-403(由于是同相放大,所以这个时候应该是11倍,不过个人认为影响不大)时,芯片发烫且无信号。可以尝试同比例扩大电阻参数,减小功率消耗。
3.至于不接匹配时自激,尝试还是接反馈电容改善。
另外,用其他运放检验是否是电路问题。。或者用一个已经测试好耳朵电路检测芯片是否坏了。。