This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[新人求助帖关于用OPA27P制作加法器的问题]

Other Parts Discussed in Thread: OPA27

用OPA27做同相加法器Vo=Vi1+Vi2的时候,函数发生器给Vi1输入频率为1kHZ,Vpp=1V的正弦波,而Vi2接地时,没有输出。然后稍作改动,成了Vo=-(Vi1+Vi2),如下图所示。虽然用函数发生器分别向Vi1和Vi2输入频率为1kHz,Vpp=1V的正弦波时实现了Vo=-(Vi1+Vi2),但是将Vi1 和Vi2的频率都改为6500Hz时,输出衰减到最大值为500mV多,而OPA27的GBW为8MHz的。求解答!!

  • 增益带宽积适用于小信号模型的情况下一般500mV以下,这边1V的正弦波属于大信号了,应该用上升斜率这个参数来计算

    外围电阻值过大。因为运放+-端是由等效输入电容的,这么大的电阻和电容形成RC低通,进一步降低信号幅度。建议用1k左右的值。

    下面我用TINA仿真了一下,大概值是对的,因为这边相当于放大了两倍,带宽变为一半了,所以幅度很低,同时等效输入电容仍然在起作用。

  • 那,请问反相加法器的带宽怎么算?