Part Number: PGA281
问题一:PGA281它是放大模拟信号的,哪些管脚确定必须要连接到数字电源和数字地。
问题二:PGA281的数字信号是用来干嘛的,它不是用来处理模拟信号吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
PGA281它是放大模拟信号的,哪些管脚确定必须要连接到数字电源和数字地。
几个增益控制引脚G0~G4都是数字引脚,它们的高低电平需要接到数字电源DVDD和数字地VSON。
PGA281的数字信号是用来干嘛的,它不是用来处理模拟信号吗?
对于PGA281来说,G0~G4的高低电平用来控制增益的,这是一款可编程增益放大器, 通过对G0~G4的高低电平配置来是实现不同的增益。参考Table1 的增益控制。
VSOP引脚的定义:Positive output-stage low-voltage supply 就是说它连接到模拟电源引脚吗?
是的,您的理解是正确的VSOP 是模拟电源。低压模拟输出级的供电电压VSOP和VSON。VSON的电压范围为VSN~(VSP)-5V。大多数情况下,VSON接GND,并且VSON作为数字地。
数字电源DVDD和数字地VSON。