This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA858: 放大器论坛

Part Number: OPA858


您好

  opa858做跨足放大器,当信号较强是858饱和后,输出信号的上升沿会有抖动。拖尾比较长,信号强度变化是宽度变化跳变,如附件所示,这是什么原因造成的呢?为什么会有这么长的拖尾呢?

谢谢

  • 您好,

    输入信号是什么?所附波形图是电路图中哪个节点的信号?可以显示出所附信号的幅值信息吗?

    当信号较强是858饱和后,输出信号的上升沿会有抖动。

    很抱歉,没明白这里的意思,OPA858输出饱和后,输出幅值应该受供电电压限制在固定值,为什么说输出信号的上升沿?

  • 输入是电流信号(APD),附图是R51位置的信号。是一个偏置3.5V的负脉冲信号。视频中,858饱和后是这样的信号吗?因为是负脉冲,所以说上升沿。R55电阻用错了吧?

  • OPA858饱和后输出就削顶了,为什么还有上升沿?您可以同时附上输入电流和输出电压的波形吗?对比看输出电压是否在随输入电流在变化?

    R55电阻和R29电阻是对5V的分压以形成3.5V的偏置电压,这里和您说偏置3.5V是一致的。