This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

微弱信号检测

当信号源电压输入是2v时,调节可调电阻5k,满足显示的电压vpp2.04v,vMax为1.02v,波形稳定为正弦波,当输入信号的电压调节到200mv时 ,显示的vpp为172mv  vMax为84mv   波形不稳定。参考信号是vpp为1v  频率为1000hz的正弦波  ,怎样调节才能使200mv时  显示的vpp为200左右      vMax 为100mv左右   在2v时也能满足vpp为2v左右  vMax为1v左右。               噪声源满足要求,均方根为1v。

  • 亲,有噪音的检测,首先要设置滤波环节。无论是用硬件还是软件。只有这样,后面电路才能看清真面目。

    因此,建议亲修改一下电路。建议参考巴特沃夫滤波器,可能对亲有些帮助。