供电24VDC 用在压力传感器上,想要4-20mA输出的配套电路方案。可编程的放大器中的程序该怎么编程。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
供电24VDC 用在压力传感器上,想要4-20mA输出的配套电路方案。可编程的放大器中的程序该怎么编程。
你好!
可以参考 PGA309 + XTR115 方案:
《Using the XTR115 with the PGA309 to Generate 4mA to 20mA Output》
可以将将配置信息存在EEPROM中:
可不可以选用PGA308和XTR116搭档呢,价格上是不是有优势?
您好,能否给个PGA309的开发工具的型号?
就是能给PGA309芯片写程序的工装。
买了个型号为PGA309EVM-USB的工装不能做生产使用,只是能做演示用,所以想买个能做生产使用的工装。谢谢!
生产使用的工装价格大概是多少?