各位专家好,请问当要放大一个方波信号时,放大器的带宽该如何确定,比如要放大一个1M的方波信号
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好XP,感谢你的解答,还有一个疑问:
比如说我要将一个100mVpp 1Mhz的方波放大十倍,那么能达到要求的运放的带宽是怎样的(跟上升沿的要求有关吧),能给我举个例子嘛
假设保留到11次谐波,那么带宽需求就是1MHz*10倍*11=110MHz,实际上这边的信号已经属于大信号了,所以就需要取决于压摆率了。这边压摆率计算可以先假设需要的方波上升沿时间为50ns,那么压摆率需求就是1V/50ns = 20V/us