看了几遍关于全差分放大器的电阻配置,感觉好晕啊,哪位好心人能把详细过程写一下呢,我用的是LMH6552,现在增益要20dB,然后是单端输入,信号源阻抗为50欧姆。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好Andy Tan,这篇文章我看过,学到一些东西,但是对于参数的配置还是不是很明白,请问能详细讲一下吗,或者私聊,这个问题困扰我很长时间了,但是一直没有解决,帮助我一下吧
根据手册中的例子,假定 RS= 50Ω,电路增益要求为 2。 此外,约500Ω反馈电阻值是一个高速放大器的合理选择。
使用这些假设,选择 R1 =249Ω和 R3 = R1 – RS || RT
根据式2,我们可以算得:
RT=58.7
所以,R3 = R1 – RS || RT=249-50||58.7=249-27=222
根据式3,我们可以算得:
R2=R4=G[R1*(RS+RT)/(2RT)]=2[(249*(50+58.7)/(2*58.7)]=461