This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ivc102芯片噪声问题

Other Parts Discussed in Thread: IVC102

您好,我使用了贵公司代理的BB公司生产的ivc102积分芯片将光电检测器的电流信号积分成电压信号,当我将芯片一直保持在s1断开,s2闭合的reset状态下时,测得的输出噪声有20mv,远大于手册上的100uv,请问是什么原因造成的?附件是我的电路图,我们也试过用贵公司的运放OPA128来设计,检测器的暗电流为3nA,使用的反馈电阻5M欧,反馈电容30pf,噪声还是有20mv左右,请问如何将该噪声降低到10mv以内呢?附件有原理图。

 

原理图.rar
  • kaili

    你好!

    能否做几个个简单的测试:

    1、你是用示波器测量噪声的吗?示波器档位(X1、X10)?带宽限制?

    将示波器表笔和地线夹子短路,此时的噪声电压峰峰值是多少?

     

    2、对于ivc102的电路,将pin1接地,开关S1开路,开关S2短路,测一下输出噪声峰峰值是多少?

    3、对于opa128电路,将电阻R1减小(例如1MOhm),测量一下输出噪声,和原来输出噪声相比是否有变化?

  • 用的是什么测量工具?不同电路噪声都在20mV左右,更像是测量方法的问题。