This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用AMC1302时,AMC1302的失调电压达到2.8mV,影响了其后端的信号处理电路,观看手册Vos典型值仅为2.5uV,如果乘以增益41,也就0.1mV,实测6个PCB板的输出失调电压都为2.8V,就算失调电压都达到手册所写的50uV,但是也不可能6个板子都处于最坏的情况吧。很困惑。原来也使用过AMC1302但也是没有达到这么大的失调电压。
您好,
您是怎样测量的输出失调电压达到了2.8mV?测试电路和输入信号是怎样的?
输出失调电压还与PSRR、CMRR、输入失调电流等参数有关,具体见链接:https://e2echina.ti.com/support/amplifiers/f/amplifiers-forum/20238/-part10-dc-error
所以还请附上您的测试电路和供电电压的纹波信息。
我没看明白AMC1302前端 R49D,R48D是怎样与R32D和R29D这个电路连接的,您可以给出它们的完整连接电路图吗?