This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,紧急求助
亲;原则上;任何运算放大器都可以单电源工作。只要注意满足输入口偏置条件即可。
参考数据手册的推荐电路
推荐电路里没有啊
为获得一个线性增益输出,VCA应该是不能在单电源下正常工作的。
下面的仿真结果,供参考:
Vin =200mv,设定的最大增益Av_max=20dB,
VF1:单电源+5V下, VG vs Vout
VF2:双电源+-5V下,VG vs Vout
上图是单电源(VF1)与双电源(VF2)下,它们的幅频特性和相频特性对比。
Vin_PP =200mv,设定的最大增益Av_max=20dB,
如果单电源采用12V的,可以达到线性增益的效果吗?