Other Parts Discussed in Thread: XTR111
描述:XTR111电路如图,参照的是手册的图36。
Q2用的是MMBT5087,Q1用的是BSP170P L6327。和demo板上的一样,PCB布局参照demo板布局。
现在测试。5脚5V,4脚接近6V。2脚9.8V,3脚9.6V。8脚4.9V。晶体管发射极和基极之间的R15上无压降。BSP170P的1,3脚有-0.22V的压差,2脚电压为0,没有输出。
问题:1. 看手册上说2脚IS电压应该比VSP低1.4V?是不是我理解错了?
The XTR111 delivers the precise output current to the IS pin. The voltage at this pin is normally 1.4V below VSP.
2. 8脚没有输出低是不是说芯片正常工作了?没有输出是因为BSP170P没有导通。
3. 4.5脚是不是往外供电的?如果我不需要往外供电的话,是不是可以不接?