This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3601: 关于最低比较电压的阈值

Part Number: TLV3601


您好专家,

我们将要调理一个信号。信号是一个上升沿在5 ns左右的脉冲信号,此信号的重频和最小周期是200 kHz。电压幅值的动态范围不超过3 V。我们的目标是当此信号过零时,就通过比较器输出一个调理后的固定幅值的脉冲信号。所以想请教一下TLV3601对于过零比较时的最小阈值电压是多少?另外是否有推荐的过零比较电路基于TLV3601.

谢谢!

  • 您好,

    TLV3601有最大5mV的输入失调电压,因此如果将阈值电压设置在0V,最大会有±5mV的误差:

    没有特别推荐的电路,过零电路的话,输入信号应该是双极性的,那么TLV3601就需要使用双电源供电,请确保输入信号幅值在TLV3601参数要求内,TLV3601是轨至轨输入的。