Other Parts Discussed in Thread: OPA454
电路具体参数如下:
Rs=1k,Rf=1k,Rp=1M,Rload=5k,去耦电容使用的是0.1uF,100V耐压,X7R.
当Vin=40V时,Vout波形会产生振荡,示波器观测Vout对地
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OPA454
电路具体参数如下:
Rs=1k,Rf=1k,Rp=1M,Rload=5k,去耦电容使用的是0.1uF,100V耐压,X7R.
当Vin=40V时,Vout波形会产生振荡,示波器观测Vout对地
你好,作为电压跟随器使用,本身运放是最容易不稳定的。而且Rf并联小电容的超前补偿是没有作用的(由于反馈环路不能产生补偿零点)。
你可以尝试以下两点建议:
1:输出端用一个50Ω以下的电阻进行隔离,这样可以隔离输出端的杂散电容。
2:增加一个10uf的大的去耦电容。由于你的负载电流较大,因此运放需要很好的去耦,以防止负载电流对运放供电的影响。
3:运放供电采用一个10Ω的电阻进行阻容隔离。
4:采用反相跟随。Gain=-1
这个是OPA454的datasheet中的负载电容与过冲的曲线图,图中可以看出该运放对负载电容是很敏感的。100pf时50%的过冲此时相位裕度大概只有20°(很容易不稳定!)