This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

跪求指导:实现455kHZ的光电漫反射通讯,通信距离5m左右,目前做了很多实验,但是光电发射和接收的频率,都到不了455k

Other Parts Discussed in Thread: OPA847, LMP7721, LMC662, OPA657

方案1:OPA847(>3GHZ)+接收管TEMD1020(上升沿4ns,下降沿4ns) 发射管9018+VSMB2020(上升沿15ns下降沿15ns).

实际测试,跨阻放大器输出端接收到的455kHz波形幅值衰减严重(Rf阻值510欧,无补偿电容),已经变成电容充放电的波形。

按照455k平率算周期2.2us,发射管接收管运放的理论值远远大于455k,为什么实际操作出来和理论值差的太远了。                                                                                                                                                                                                         

  • 我看才 455KHz.. 有那么困难吗?

    能否上个电路, 分析一下

  • 亲,相应与外围及封装PCBLayout都有关,上传个电路和PCB,让我们看看到底啥问题。

  • 上传一下你的原理图和PCB,运放本身的带宽足够,和外围电路参数有关系

  • yan bo 说:

    方案1:OPA847(>3GHZ)+接收管TEMD1020(上升沿4ns,下降沿4ns) 发射管9018+VSMB2020(上升沿15ns下降沿15ns).

    实际测试,跨阻放大器输出端接收到的455kHz波形幅值衰减严重(Rf阻值510欧,无补偿电容),已经变成电容充放电的波形。

    按照455k平率算周期2.2us,发射管接收管运放的理论值远远大于455k,为什么实际操作出来和理论值差的太远了。                                                                                                                                                                                                         

     电路如图,就是最普通的iv放大,光电接收管用的vishy的,LMC662和lmp7721测灵敏度,效果很好,可是频率率上不去,实际测试中C8,C2 都没有加。R2,R12从1G到510欧姆都试过。

  • 把R4和R14这两个1M电阻减小,用1K尝试一下

  • 现在Rf用50k,1M电阻去掉,455k漫反射通讯距离只有1m,要想增加通讯距离有没有什么建议?

    目前想到如下方案:

    1.加大发射功率,增加漫反射距离。

    2.更换LMP7721运放,采用增益带宽更高的运放,OPA847,OPA657 增大Rf,提高弱电流的增益。

    3.加一级低电压噪声放大,在进行带通滤波,在放大。