This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,所谓的隔离几千伏电压是指输入和输出之间,而你所说的输入电压范围是针对输入与VDD1之间,输出与VDD2之间
你好,你说的对,如果VDD1=5V, 那么VINP 和VINN会受到限制;而VDD1和VDD2之间是不共地的,可以有很高的隔离电压差,就是你说的几千伏的级别
你好,VDD1和GND1之间最大压差为6V,所谓的几千伏是指输入和输出间,也就是VDD2对于GND1可以到几千伏,你可以仔细阅读一下手册和隔离的概念